To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Now Stocks Waterproof USB 3.0 Cable Assemblies for Harsh Environment Applications

Tuesday, March 24, 2020

L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of IP67- rated waterproof USB 3.0 cable assemblies for use in test and measurement, data transfer and harsh environment computing applications.

L-com’s new waterproof USB cable assemblies are USB 3.0 compliant and feature a waterproof, panel/enclosure mount connector on one end of the assembly. These rugged cables boast threaded couplings and O-ring seals that ensure IP67-rated protection from water and dust. Rugged, molded backshells deliver durability and 30-micro-inch gold-contact plating provides a reliable connection even with repeated mating cycles. Off-the-shelf configurations include waterproof USB-A-male to standard USB-B-male, waterproof USB-A-female to standard USB-A-male and waterproof USB-B-female to standard USB-A-male options.

Additionally, shielded versions are offered that employ a metal coupling nut that provides a 360-degree shield when mated with a metal, female L-com U3A cable assembly. Shielded, waterproof USB cable options include shielded waterproof USB-A-male to standard US-B-male and shielded waterproof USB-A-male to standard USB-A-male assemblies. What is USB-A? Read our blog post for more info.

“The addition of these new IP67-rated USB 3.0 cables adds to our extensive line of waterproof USB interconnects and provides our customers with even more options when dealing with USB connectivity in unforgiving environments. Furthermore, since the new assemblies are USB 3.0 complaint, they are able to handle up to 4.8 Gbps data rates to address today’s high-speed computing applications,” said Dustin Guttadauro, Product Line Manager.

L-com’s new waterproof USB 3.0 cable assemblies are all in-stock and available for immediate shipment.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, ShowMe Cables, INC-Installs and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936