NORTH ANDOVER, MA - 2/5/15 - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, has released a series of
embedded PCB antennas to address OEM and ODM wireless device applications.
L-com's HyperLink® brand embedded antennas are designed to directly integrate with devices that require wireless capabilities. By embedding these PCB antennas directly into a device, the need for an external antenna is eliminated.
The new embedded antennas include support for 2.4 GHz, 4.9/5.8 GHz and dual band 2.4/5.8 GHz operation, and feature integrated low loss 1.13 mm coaxial leads that are terminated with U.FL/IPX connectors.
"L-com is excited to offer these types of embedded antennas to the industry. Our ability to custom design these PCB antennas will certainly aid engineers who design devices that require wireless capabilities," said Ken Burgner, Product Manager.
The three new antennas have been specifically designed to provide customers a quick embedded antenna solution. In addition to these standard antennas, L-com can custom design embedded antennas to meet customer's specific design requirements. This includes custom shapes and sizes; multiple connector options, such as MMCX, U.FL and SMA, and frequency and gain options.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/