To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Offers New 4-Way Signal Splitter for Wideband WLAN Applications

Tuesday, July 21, 2009
North Andover, MA – July 22, 2009 –  L-com, a global leader in the manufacture of wired and wireless connectivity products today announced the release of the SCW04N 4 way wireless splitter to address wideband WLAN applications.  The SCW04N is a 4-way wideband signal splitter which covers a frequency range of 750 MHz to 2700 MHz. This wideband design makes this signal splitter suitable for 800MHz & 900 MHz cellular and ISM band operation, 1.8 GHz & 1.9 GHz (1800-1900 MHz) PCS cellular radio applications, as well as 2.3 GHz WCS Band (2.31 - 2.36 GHz), 2.36 GHz CDMA Band and 2.4 GHz 802.11b, 802.11g and 802.11n applications.

This signal splitter features a 50W power rating and is constructed from heavy duty aluminum. The SCW04N is designed to be installed indoors or in a weather-resistant enclosure.

   

For more information about this release, please contact:
Ken Burgner , Product Manager
561 -995-2256 x7140, kburgner@l-com.com

About L-com 

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com