![]()
NORTH ANDOVER, MA - 02/17/14 - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has expanded its line of rack mount lightning and surge protectors to include 12-port and 24-port models, in addition to its 4-port models.
L-com's RMSP series rack mount protectors span a variety of types including Cat 5, Cat 6, and DSL/ Telephone/T1 models. Each unit provides superior lightning and surge protection to help prevent damage to expensive network equipment.
"Many of our customers inquired about providing multiple line protection. The 12 and 24 port protectors allow them to maintain flexibility and integrate protection into their existing racks," said Ken Burgner, Product Manager.
The new 2U 12-port protectors are constructed from 1/16" thick cold rolled steel and are flat black powder coated. These models can be used with L-com's PR-CMB Cable Management Bracket Kit. The new RMSP-CAT5-24 is a completely self contained 24-port protector in a 1U rack mount enclosure. It features a built-in rear cable management rail.
New Product Details:
The RMSP-CAT5S-12 provides protection for up to 12 Cat 5 data lines.
The RMSP-CAT5-24 provides protection for up to 24 eight Cat 5 data lines.
The RMSP-CAT6-12 Surge Protector provides surge protection for up to 12 Ethernet lines using 10/100/1000 data rates.
The RMSP-CAT6T-12 lightning and surge protector provides superior lightning and surge protection for up to 12 lines with improved frequency response for indoor 10/100/1000 Ethernet networks.
The RMSP-DT-12 is a high performance 3-stage lightning protector that provides superior protection for up to 12 DSL, Telephone and T1 lines from transients and surges. It is designed to convert into a failsafe mode in the rare case of a catastrophic surge or lightning event.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/