NORTH ANDOVER, Mass. (November 19, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has developed two MIMO sector antennas that provide true 180-degree coverage.
L-com’s HG2458-13P-180 is a 180-degree dual-band MIMO sector antenna that combines high-gain and dual-band support for applications in the 2.4 GHz (2400-2500 MHz) and 5 GHz (4900-5850 MHz) frequency bands.
“The HG2458-13P-180 stands out from our competitors sector antennas because it is a true 180-degree dual-band sector antenna that features patent pending technology,” said Ken Burgner, Product Manager.
The HG5813DP-180 is a 180-degree dual-polarized MIMO sector antenna. It delivers high-gain with vertical and horizontal polarization for applications in the 4.9 GHz to 5.8 GHz frequency bands.
“The HG5813DP-180 features the same patent pending technology as the HG2458-13P-180. This technology enables it to provide true 180-degree coverage in addition to dual-polarization,” added Burgner.
Both of these antennas feature a dual-feed system via two integral N-Female connectors. The HG2458-13P-180 antennas utilize a separate feed for 2.4 GHz and 5 GHz bandwidths. The HG5813DP-180 offers separate feeds for horizontal and vertical polarization.
These antennas feature heavy-duty UV-resistant plastic radomes for all-weather operation. Additionally, they are supplied with a stainless steel tilt and swivel mast mount kit, which allows installation with various degrees of up/down tilt for easy alignment.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/