NORTH ANDOVER, MA, -- June 12, 2009 -- L-com, a global leader in the manufacture of wired and wireless connectivity solutions, has released new series of 2.4 GHz 5 dBi Spatial Diversity antennas for indoor WLAN applications requiring wide area coverage.
The HG2405SD-135 series HyperLink brand antennas feature dual independent Dipole radiating elements for Spatial Diversity. This new antenna can be used in 2.4 GHz IEEE 802.11b/g/n applications and is an ideal match for access points with dual diversity ports. It can be installed for vertical or horizontal polarization and is available in multiple configurations of cable length and connector type. The most popular configurations are available off the shelf. Custom versions are available within days of placing an order.
The HG2405SD-135’s aesthetically appealing design is a compact 3.2" X 6.2" X 2.2" and uses a durable UV-stable white ABS radome. The 135° horizontal beam-width makes this antenna a perfect solution for coverage in large open space WiFi applications such as office and Hotspot applications.
Units will be available for shipping in late June 2009.
For more information about this release, please contact:
Karl Blomgren, Product Manager
561.995.2256 x7183, mailto:kblomgren@hyperlinktech.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com