NORTH ANDOVER, Mass. (March 24, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new 4G/LTE amplifier.
L-com’s HA72170-NF 4G/LTE booster is able to capture a weak cellular signal and strengthen it to provide crystal clear calls and fast, consistent data speeds while reducing the number of dropped calls. The HA72170-NF booster can wirelessly connect more than 25 mobile devices and works with 2G, 3G and 4G networks on all major US cell carriers. The LED control console on the booster allows the user to set the operational mode, select a band, and adjust the gain of each frequency.
“An increasing number of devices depend on a reliable cellular signal for voice service and data. Dropped calls, slow data speeds and shortened battery life are just some of the issues related to weak cell signal. Our 4G/LTE booster can take a cellular signal and amplify and rebroadcast it from within a building or structure to provide better connectivity for cellular subscribers,” said Ken Burgner, Product Manager.
The HA72170-NF 4G/LTE booster is FCC certified and features automatic gain control for consistent coverage. The LED console display indicates signal levels and makes installation quick and easy. Kits are available with indoor and outdoor antennas and coaxial cables in lengths of 25, 50 and 75 feet.
L-com also offers products such as indoor and outdoor HyperLink brand wireless antennas, low-loss coax cabling and surge protection devices.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/