L-com Releases 5-Port and 8-Port Gigabit Desktop Switches ![]() | LC-SW805G (5-port version) Front | ![]() | LC-SW805G Back (8-Port Version Not Shown) | NORTH ANDOVER, MA - 08/01/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added two gigabit Ethernet switches to its lineup of commercial Ethernet products. The new products are backed by L-com's high-quality brand and offered at very competitive prices. As LANs evolve from 10/100 to 10/100/1000 Base-T able to handle up to 1 Gbps speeds, network components including switches for the higher speeds are in increasingly high demand. This is the first time L-com has released a commercial switch for this application, though they have carried industrial-grade Ethernet switches since 2011. With the 5-port and 8-port options priced at around US$35 and US$45, respectively, these new switches are a price-sensitive option that comes with L-com's brand reputation. "There is a great need for networking devices that are compliant with gigabit networks," said Manuel Martinez III, Product Manager. "I'm happy that we're able to support this with high-quality products at budget-friendly prices." The new switches come with auto-negotiation, auto-MDI/MDIX, and support for up to 8k absolute MAC addresses. The datasheets and user manuals are available for free download from L-com's website. For high-res versions of these images suitable for print publication, please follow these links, right click on the image, and select Save As: https://www.l-com.com/lcom_emails/2013/072913/LC-SW805G-back-lg.jpg https://www.l-com.com/lcom_emails/2013/072913/LC-SW805G-front-lg.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |