L-com Releases a 48VDC All-In-One PoE Injector with 24W Power Supply ![]() NORTH ANDOVER, MA - 9/20/12 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added a wall mount 48VDC all-in-one Power-over-Ethernet (PoE) injector. This item joins the rest of the all-in-one PoE line that L-com first introduced in August. The all-in-one PoE injectors are designed to simplify PoE setups and minimize their space requirements by eliminating the need for a separate power supply. Among the wall mount items introduced in August were a 12VDC unit and a 24VDC unit. Most radio products like wireless access points and bridges require 48VDC, however, which L-com only covered with desktop models. This new wall mount model is ideal for tight spaces such as L-com's 120VAC Industrial enclosures or AC Universal Outlet enclosures since it can convert them into a 48VDC PoE ready enclosure. "We immediately recognized a need for a wall mount 48VDC product for our all-in-one line," said Patrick Pesa, Director of Product Development. "We quickly designed a model to accommodate the wireless radio applications that we already support with antennas, cables, and enclosures." The new PSW4824-POE is set to be available to ship in October, 2012. L-com has posted a datasheet, pinning diagram, and 2D engineering drawing of this item for free download from their website. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com To download a high-resolution version of the image for this press release suitable for print publication, click this link: https://www.l-com.com/lcom_emails/2012/092012/PSW4824_POE.jpg L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |