NORTH ANDOVER, MA – 05/21/2010 – L-com is pleased to introduce its new line of AISG compatible products for use with Remote Electrical Tilt (RET) antenna systems.
These new products include the following:
Lightning Surge Protector The HGLN-AISG1 high performance 3-stage lightning/surge protector provides surge protection for indoor and outdoor control units and outdoor antennas. The protector is compatible with AISG 5, 6 and 8-conductor control lines and provides individual protection of the Power and RS485 lines within the control cable. |
Connectors These FS1 type 8-pin screw coupling connectors are available in Male and Female versions. They are designed according to DIN 45326 standard and are EMI protected and IP67 rated. Designed for use with 5, 6 or 8-conductor AISG type control cable, these connectors feature solder cup type pins and an internal clamping system that helps ensure the connector is securely attached. |
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/