To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases DB25 Connector for Field Terminations

Monday, June 2, 2008

North Andover, MA – June 3rd, 2008 –L-com has released a new, easy-to-use DB25 Field Termination Connector which is perfect for quickly terminating data cables in the field. This exclusive L-com design features separate connection points for all 25 positions of the connector plus the ground and no soldering or crimping is required. The terminal block utilizes set screws which provide reliable electrical connections requiring no special tools. The DGB25FT is panel mountable for thickness up to 0.062".

 

For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x156, ssmith@l-com.com

About L-com

Founded in 1982, L-com is a privately held Massachusetts Corporation, dedicated to the design and production of a wide range of interconnect products for the electronics and data communications industries. Primary product emphasis is placed on copper and fiber cable assemblies and accessories for modular and coaxial applications as well as computer networking. The company endeavors to serve the industry by offering solutions to interconnect problems. This effort has led to the development of many new products, some of which are proprietary. L-com has also introduced switching and testing devices in each of their basic product areas. Products are marketed domestically and internationally.