NORTH ANDOVER, Mass. (August 25, 2016) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a flexible embedded antenna.
L-com’s HyperLink brand HG72705FPU-UFL is a flexible, Omni-directional embedded antenna designed to be directly integrated into devices that require wireless capability. By embedding this antenna into a device, the need for external antennas is eliminated. The Omni-directional design of the HG72705FPU-UFL provides complete 360° coverage, making it ideal for multipoint and mobile wireless systems.
The HG72705FPU-UFL is specifically designed for Distributed Antenna Systems (DAS) used to distribute cellular and Wi-Fi signals throughout a building or area. With an operating range of 698-960 MHz to 1710-2700 MHz, it is ideal for cellular LTE and Wi-Fi applications. The multi-band capability of this antenna eliminates the need to use different antennas for each frequency.
”Today’s antennas need to be small enough to embed into smaller devices yet powerful enough to operate on a wide range of frequencies that include cellular, Wi-Fi and even DAS networks. The HG72705FPU-UFL was designed as a quick off-the-shelf solution and is ideal for engineers developing prototype equipment that requires an antenna for devices with tight space constraints,” said Ken Burgner, Product Manager.
Constructed from a flexible polymer, the HG72705FPU-UFL can be attached to flat or curved surfaces by its adhesive backing. This unique design provides engineers with greater flexibility when designing wireless communications equipment.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking equipment, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions, Aiconics®, a leading manufacturer of electrical connector products and Point Six™ Wireless, pioneers in the design and manufacture of wireless sensors used in IoT applications. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:
https://www.L-com.com/