NORTH ANDOVER, Mass. (September 24, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has developed the industry’s first 802.11ac 4x4 MIMO outdoor Omni directional, dual polarized / dual frequency antenna line, which features patent-pending technology.
The HyperGain® DPU series antennas can operate in both vertical and horizontal polarization. Dual polarized antennas are often used with MIMO/802.11ac devices to enable multi-stream communication. This allows the device to transmit data on one polarization while simultaneously receiving data on the other. Dual polarized antennas enable multi-stream communication through one antenna instead of using two independent (and opposite polarized) antennas for the same result.
This technology also supports the attenuation of unwanted signals from adjacent channels and/or co-located equipment, thus improving RF performance and increasing data speed. Supported MIMO types include 2x2 systems (two streams), 3x3 systems (three streams) and 4x4 systems (4 streams).
“Quad” Omni antennas are actually four antennas in one package. They feature separate horizontal and vertical elements for the 2.4 GHz frequency band and another set of horizontal and vertical elements for the 5 GHz frequency band. The internal elements are accessed via four individual N-female connectors.
“We are proud to announce these industry-first MIMO antennas. Our patent-pending design allows our customers to realize faster data rates and less RF interference than the other MIMO antennas that are currently available on the market," said Patrick Pesa, Director of Product Management. “Additionally, these antennas are backward compatible with 802.11n networks and will support future 802.11ac Wave 2 applications” said Pesa.
The new antennas are available in 6, 9 and 11dBi gain and feature UV resistant PVC radomes that ensure years of reliable operation in all weather conditions. Additionally, the heavy-duty extruded aluminum base allows these antennas to be mounted on masts of up to 3.7 inches in diameter.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174,
mailto:pmcneil@l-com.com About L-com Global Connectivity
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit:
https://www.L-com.com/