NORTH ANDOVER, MA – 5/6/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today the release of a new series of IP67 rated RJ45 Industrial Ethernet cables, panel mount IP67 RJ45 jacks (feed-thru and 110 styles), and IP67 long and short body RJ45 strain reliefs. These IP67 rated products are designed for use in harsh environments where dust and moisture are present.
- The TRD5WP cable series features UV and chemical resistant PUR jackets as well as shielding to protect against EMI/RFI.
- The WPRJ series panel mount jacks feature straight and 90 degree shielded feed-thru options as well as a 110 style punch down version.
- The WPRJ-XSR series features long and short body IP67 rated strain reliefs which can be used to build your own IP67 rated Industrial Ethernet cable assemblies.
“Our new IP67 series of cable assemblies and panel mount jacks were created to address the ever growing Industrial Ethernet market. By offering these high quality, competitively priced IP67 products, we have further enhanced our already extensive line of IP rated Ethernet products. By giving our customers more choices we are able to address new application requirements.” said Peter McNeil, L-com’s Telecom Product Manager.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/