To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases IP68 Fiber Plugs, Receptacles and Jam Nuts

Monday, July 24, 2017

NORTH ANDOVER, Mass. (July 25, 2017) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of LC fiber plugs, receptacles and jam nuts to address high speed voice, video and data networking applications.

These new IP68 rated fiber products were designed to stand up to extreme environments while providing high throughput network connectivity. The ruggedized IP68 fiber plugs and IP68 fiber receptacles offer 400lb pull strength and 450lb crush resistance as well as protection from moisture, liquid and dust. Both plugs and receptacle are available in Multimode, Single mode, and APC polish Single mode types.

In addition to the new LC plugs and in-line receptacles, we now offer IP68 rated flange mount, jam nut, D38999 and daisy chain style fiber receptacles that are perfect for mounting to an enclosure or panel. These receptacles are also offered in Multimode, Single mode, and APC polish Single mode styles.

“These new IP68 fiber plugs and receptacles were designed to take a beating while offering optimal network performance. They are perfect for industrial networking applications involving fiber where exposure to chemicals, physical contact and the environment are prevalent, “said Dustin Guttadauro, Product Manager.

These new IP68-rated fiber LC plugs and receptacles are in stock and available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: