To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases IP68-Rated USB 2.0 Cable Assemblies and Panel-Mount Coupler

Wednesday, January 16, 2019

NORTH ANDOVER, Mass. (Jan. 17, 2019) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has released a new line of IP68-rated, USB 2.0 cable assemblies designed for use in harsh environment connectivity applications.

The new U3A00064-series cables feature a USB 2.0, Type-C, waterproof, IP68-rated connector on one end of the assembly and a standard USB 2.0 Type-A connector on the other end. Additional features include gold-plated contacts that stand up to repeated mating cycles, 32/24/28 AWG cable and double shielding to reduce the effects of EMI/RFI.

In addition to the new U3A00064 cable assemblies, L-com has also introduced a new waterproof, panel-mount, Type-C connector with PC tails that is also IP68-rated. The U3B00001 features threaded couplings and an O-ring seal ensuring protection against water and dust. 

“The addition of these new IP68-rated USB connectivity products complements our extensive line of waterproof USB interconnects designed for use in harsh, demanding environments. These new products address the growing need for USB Type-C applications that are now being implemented in harsh, industrial applications, “said Brian Gates, Product Manager.

L-com’s IP68-rated USB 2.0 cable assemblies and IP68-rated Type-C panel mount couplers are in stock and available for immediate shipment.

For more information about this release, please contact:

Peter McNeil
L-com Global Connectivity
17792 Fitch
Irvine, CA
978-682-6936 

About L-com Global Connectivity:

L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Infinite Electronics is a leading global supplier of electronic components serving the urgent needs of engineers through a family of highly recognized and trusted brands.  Our portfolio brands are specialists within their respective product set, offering broad inventories of engineering-grade product, paired with expert technical support and same day shipping. Over 100,000 customers across a diverse set of markets rely upon Infinite Electronics to stock and reliably ship urgently needed products every day.

Search Entries: