NORTH ANDOVER, MA – 3/4/10 – L-com Global Connectivity, a leading manufacturer of both wired and wireless connectivity products, announced today the release of new AC/DC Control Line protectors. These high power 3-stage Lightning and Surge protectors, which come in 12V, 24V, and 48V, provide superior protection of control lines from transients and surges.
Like many of L-com’s other Lightning Protectors, these come with removable screw terminal strips for fast and easy setup, and a ground clamp provided on the outside of the enclosure for easy grounding. Each Lightning Protector is able to protect up to 8 individual single ended control lines.
Lightning protectors are designed to protect vulnerable equipment from power surges, like what equipment would experience in a lightning strike. Power surges are an obvious problem in outdoor antenna installations, but they are a growing problem for indoor installations as well. L-com now carries nearly 100 different lightning protectors, and with their custom program they can manufacture special versions, making their offering a one-stop shop for surge protection of every kind.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450,newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/