NORTH ANDOVER, MA - 04/24/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that they have released further line of space-saving options for D-Sub applications with their new 90° angled D-Sub cable assemblies. These 90° D-Sub cables are designed for use in enclosures, cabinets or other confined-space applications where standard straight D-Sub backshells will not fit.
"As we've discovered with Ethernet, HDMI, USB and other cable types, our angled cable assemblies are becoming more and more popular with engineers and systems designers," said Steve Smith, Product Manager, "The 90 degree angle gives our customers the flexibility they need for confined space applications."
Each series offers four angle options, various cable lengths, and are available in DB9, DB15 and DB25 sizes. These rugged cable assemblies feature a straight D-Sub connector on one end and a 90° left, right, up or down exit D-Sub connector on the other. Custom versions can be manufactured with modest minimum requirements.
L-com's new D-Sub cables also utilize 360° shielding for protection against EMI/RFI and molded backshells which provide durability and increased strength at the cable entry point. Applications for these D-sub cables include RS232 serial communications, test and measurement applications, uninterruptible power supply communications and data networking. The RJ45 to DB9 connector can be used for backwards compatibility.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###