NORTH ANDOVER, MA - 07/03/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, announced today that as a result of the success of their existing dual band flat panel antennas, they have added two new models to their DP series of dual polarity 2.4/5 GHz flat panel antennas. The new HG2458-10DP-6NF and HG2458-14DP-4NF models combine vertical and horizontal polarization with high gain over a broadband frequency range in a single enclosure. Both models operate at 2.4/4.9-5.8 GHz, which makes them ideal for IEEE 802.11a, 802.11b, 802.11g, 802.11n and the new 802.11ac standard applications. Since they can operate at 4.9 GHz, they can also be used for homeland security and public safety band applications.
"The wide band design of these antennas has eliminated the need to purchase separate antennas for each frequency," said Kenneth Burgner, Product Manager, "They represent an innovative solution for our customer’s wireless applications."
The DP series antennas operate in vertical as well as horizontal polarization. Dual polarized antennas are often used in MIMO/802.11n applications to enable multi-thread communication. This allows the device to transmit data on one polarization and simultaneously receive it on the other. The advantage of this is that multi-thread communication can be achieved with the use of one antenna instead of using two independent (and opposite polarized) antennas for the same result.
The HG2458-14DP-4NF combines four dual band antennas in a single housing and consists of two vertically and two horizontally polarized multi-patch antennas, each fed via its own N-Female connector. The unit can be used with access points and routers with one to four antenna ports. The gain of this antenna is 13 dBi @ 2.4 GHz and 14 dBi @ 5 GHz.
The HG2458-10DP-6NF combines six dual band antennas in a single housing. The unit consists of four vertically and two horizontally polarized multi-patch antennas, each fed via its own N-Female connector. This unit can be used with access points and routers with one to six antenna ports. The gain of this antenna is 9 dBi @ 2.4 GHz and 10 dBi @ 5 GHz.
Both models also feature a heavy-duty UV-resistant plastic radome, which makes them ideal for all-weather operation. A tilt and swivel mast mount kit is included, which allows for quick installation and various degrees of up/down tilt for easy alignment.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###