To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases New Ethernet Lightning and Surge Protectors with PoE, PoE+ and PoE ++ Support

Tuesday, October 1, 2019

IRVINE, Calif. - L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of Gigabit Ethernet lightning and surge protectors designed to protect valuable communications equipment from power surges and indirect lightning strikes.

These robust RJ45 surge protectors provide effective protection against electrical transient surges that are generated by both external lightning events and by internal switching events. They also support long-term system reliability by safely shunting high amounts of transient energy while maintain­ing a very low clamping voltage.  

The LPXTRJ45-GBPOE-series surge protectors utilize state of the art GDT, SASD technology to protect critical equipment in 10/100/1000Base-T protocol data networks, while remaining transparent to data throughput and passing DC power through. Additionally, these surge protectors support PoE (IEEE 802.3af), PoE+ (IEEE 802.3at) and PoE++ (IEEE 802.3bt) Power over Ethernet applications.

“The LPXTRJ45-GBPOE-series surge protectors offer high levels of surge protection by utilizing proprietary surge technology that responds quickly to damaging power surges and indirect lightning strikes. In addition to offering support for fast Gigabit Ethernet speeds, these new surge protectors also support a variety of PoE applications,” said Dan Rebeck, Product Line Manager. In addition, check out our All-In-One DC PoE injectors with power supplies which compliment some of the other products already discussed.

L-com’s new Gigabit Ethernet, PoE lightning and surge protectors are in-stock and available for immediate shipment.

About L-com:

L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.

About Infinite Electronics:

Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, Kaelus, ShowMe Cables and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.

###

Press Contact:

Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936