NORTH ANDOVER, MA -- June 1, 2009 -- L-com, a global leader in the manufacture of wired and wireless connectivity solutions, has released three new four port 802.3af PoE injectors to address applications where multiple data/power connections are required.
The new BT-CAT5-P4 series injectors feature Industrial grade cast aluminum housings and shielded RJ45 jacks for EMI suppression. The BT-CAT5-P4-4848 ships with a 48 watt power supply and the BT-CAT5-P4-4870 ships with a 70 watt power supply. The standard model BT-CAT5-P4 does not include a power supply but can be used with a user supplied AC or DC power supply up to 60 volts.
![]()
For more information about this release, please contact:
Greg Pepin, Product Manager
978-682-6936 x1186, gpepin@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com