To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases New IP67 IEEE 1394 Firewire Cable Assemblies for Industrial Computing Applications

Tuesday, March 24, 2009

North Andover, MA – March 25, 2009 –  L-com Global Connectivity today announced the release of two new families of IP67 IEEE 1394 Firewire cables assemblies for use in industrial or harsh environments. The new WP946PXX series features assemblies with one IP67 male to one standard 6 position male connector, and another version with one IP67 Female 6 position connector to a standard 6 position male connector.

“This new series represents the first in a line of IP67 rated Firewire products for L-com. As we see the need for more industrial rated products we continually fill these gaps where such products did not exist," said David Dolce L-com’s Product Development Manager.

These assemblies are perfect for applications where dust and moisture are prevalent and can be used to connect to, enclosures, panels, or directly to peripherals or PCs.

 

 


For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com

About L-com

L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com