NORTH ANDOVER, MA – 3/11/2010 – L-com, Inc., a leading manufacturer of both wired and wireless connectivity products, today released three new Data Line Lightning Protectors designed to protect 10/100 and 10/100/1000 Base-T Ethernet systems.
Outdoor 10/100 Base-T CAT5
Lightning Surge Protector - AL-CAT5SJW
This compact weather resistant lightning surge protector is designed for use with 10/100 Base-T CAT5 Ethernet networks and is Power-Over-Ethernet (PoE) compatible. It provides protection to data lines as well as PoE DC power feed lines.
Features:
- 802.3af modes A and B PoE compatibility
- Reverse Polarity PoE compatibility
- Shielded RJ45 jacks to help reduce EMI interference
- Supports use of shielded CAT5 cable
Weatherproof 10/100 Base-T CAT5e
Lightning Surge Protector - AL-CAT5EJWP
Designed for all weather applications, this high power lightning surge protector is compatible with both CAT5 and CAT5E 10/100 Base-T Ethernet networks. Like the AL-CAT5SJW, it provides protection for data lines as well as PoE DC power feed lines. This protector is an ideal alternative to the Motorola/Transtector ALPU-ORT.
Features:
- 802.3af modes A and B PoE compatibility
- Weatherproof ABS enclosure with gasketed cover
- Shielded RJ45 jacks to help reduce EMI interference
- Superior power handling capability compared to TVS or Zener diode based designs
![]()
Weatherproof 10/100/1000 Base-T CAT6
Hi-Power Lightning Protector - AL-CAT6HPW
The AL-CAT6HPW provides superior lightning and surge protection for indoor 10/100/1000 Base-T Ethernet networks. The unit has low line-to-line and line-to-ground capacitance to minimize distortion of high-speed signals. The shielded RJ45 jacks of this protector are isolated from the safety ground which minimizes the chance of a ground loop being introduced. This protector is a superior and lower cost replacement for the Motorola PTP-LPU lightning protector.
Features:
- CAT5, CAT5E and CAT6 compatibility
- GR-1089 Intra-building rated
- Weatherproof ABS enclosure with gasketed cover
- PoE compatibility
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/