NORTH ANDOVER, MA – 3/30/2010 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, announced today the availability of a new line of Power over Ethernet (PoE) Midspan/Injectors with Integral High-Power Lightning and Surge Protection. These new products allow greater surge protection to enable peripheral items to operate in areas where lightning or power surges are common.
The new PoE line includes these features:
- CAT5e and CAT5 compatibility
- Surge Protection on all lines
- GR-1089 Intra-Building rated
- Available individually or in kits with either 48VDC @ 48W or 48VDC @ 70W power supplies
- Indoor and outdoor versions available
Ken Burgner, L-com’s Product Manager in charge of PoE, said, “We have been making and selling a variety of PoE products for several years now. The standard is no longer new, but that doesn’t mean that there is no room for innovation and increased offerings. We will continue to lead the PoE market with products and educational materials.” Among the educational materials, Burgner recommended the “What is Power-over-Ethernet?” whitepaper that is available for free from L-com’s Technical Resources page on www.L-com.com.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/