NORTH ANDOVER, MA, -- 1/20/10 – L-com Global Connectivity, a leading manufacturer of both wired and wireless connectivity products, announced today the addition of double-shielded extreme high flex Industrial Ethernet patch cords to their product offering. These new patch cords feature:
Braid and foil shield to maximize protection against EMI and RFI
Low Smoke Zero Halogen (LSZH) jackets to prevent the release of toxic gasses should the cable catch on fire
PUR jacket to resist oil and other contaminants, preventing cable jacket break down in industrial environments
Hi-Flex design which supports use in continuous movement applications
In addition to these new high flex Industrial Ethernet cables, L-com carries a host of industrial rated products including Industrial Ethernet Switches, PLCs and more.
Furthermore L-com stocks hundreds of shielded Cat 5e and shielded Cat 6 Industrial Ethernet cables to satisfy all of your industrial networking applications.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/