L-com Releases new USB UPM Style Panel Mount Cables
![]()
NORTH ANDOVER, MA - 01/30/14 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, announced today that it is now selling
USB 2.0 UPM Style Panel Mount Cables with 2mm pitch PCB Header Connectors. L-com's Panel Mount USB cables are designed to make "board-to-box" USB connections a cinch with a pre-installed 5pin 2mm pitch connector.
These USB cables are a metric addition to L-com's popular
UPMA5 &
UPMB5 cable series, which use 0.100" (2.54mm) pitch connectors. Pitch is defined as the distance between connector positions.
"We've had several custom product requests for metric versions of our existing panel mount USB cables with PCB header connectors," said Steve Smith, Product Manager. "Now they are available off the shelf."
The cable used on these assemblies is double shielded for maximum EMI resistance and the power conductors are 26 AWG to accommodate the crimp contacts. Each assembly includes two 4-40 x 3/8" Phillips pan head mounting screws. L-com also offers quantity and custom length pricing for this product.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com/