North Andover, MA – July 30, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity products today announced the release of a new panel mount USB surge protector. The new product, AL-ECF504-AB, is a commercial quality device designed to protect a computer's sensitive USB ports from surges and spikes from attached devices.
To ensure USB 2.0 speeds, the device uses ultra-low capacitance diodes to protect the data lines. In addition, a protection device clamps the power lines to safe levels. This USB surge protector is ideal for protecting a PC from USB connected devices including USB hubs, WiFi USB client adapters, and USB enabled surveillance cameras. And for an upgrade, check out our USB 3.0 powered hub which offers many advanced features.
The AL-ECF504-AB is designed to be mounted in L-com’s ECF style panels, and can also be used in custom cut wall plates and panels.
For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com