NORTH ANDOVER, Mass. December 17, 2015) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has launched a new series of UL® listed weatherproof industrial enclosures.
Constructed from molded halogen- free and self-extinguishing fiberglass reinforced polyester (FRP), these enclosures are well suited to high temperature or corrosive environments.
The NBB series enclosures are available in L-com's two most popular sizes: the NBB141207 (14x12x7 in.) and NBB181608 (18x16x8 in.).
The black color of the NBB series makes these enclosures ideal for security and surveillance equipment, since they seamlessly blend in with existing municipality landscapes. Additionally, the contoured body produces an attractive and contemporary appearance.
“Our new NBB series enclosures are perfect for applications where environmental extremes prevail. We offer many different heating and cooling options all off-the-shelf," said Ken Burgner, Product Manager. "Additionally we offer custom versions of these enclosures to address applications for both wired and wireless installations," continued Burgner.
These NEMA rated enclosures also feature fully gasketed lids and integral mounting flanges that allow them to be mounted on walls and flat surfaces without the need for extra mounting hardware. Optional pole mounting kits are also available.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, mailto:pmcneil@l-com.com
About L-com Global Connectivity:
L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink® , L-com’s other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for more than 30 years, L-com, which is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. For more information, please visit: https://www.L-com.com/