To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Releases USB 3.0 Cables with Ferrites and LSZH Cable Jackets

Monday, August 6, 2018

NORTH ANDOVER, Mass. (August 7, 2018) - L-com Global Connectivity, a preferred manufacturer of wired and wireless connectivity products, announced today that it has just released a new series of USB 3.0 cable assemblies with low-smoke zero-halogen (LSZH) jackets and ferrite beads.

Ferrite beads prevent interference from a connected device or to a connected device and help to reduce electromagnetic interference (EMI) from either being radiated by a cable or being received by a cable.

Additionally, these new USB 3.0 cables feature LSZH cable jackets and connector over molds. LSZH compound reduces the amount of toxic and corrosive gases emitted during combustion, and will self-extinguish after catching on fire.

L-com offers two versions of these assemblies. One version features USB 3.0 Type-A male to Type-A male connectors and the other version features USB 3.0 Type-A male to Type-B male connectors.

“These new USB cables with ferrites and low-smoke jackets offer multiple levels of protection while providing high-speed USB 3.0 performance. These new assemblies are perfect for data storage, streaming video and data acquisition applications,” said Brian Gates, Product Manager.

L-com’s new USB 3.0 cable assemblies with ferrite beads and LSZH jackets are in stock and are available for immediate shipment.
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
L-com Global Connectivity, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics company.

Search Entries: