NORTH ANDOVER, MA - 06/26/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, today announced that they will be adding two new mini mobile NMO antennas to their HyperLink Wireless UR and MGUR series. Available with either black or white ABS radomes, these enclosed compact antennas are ideal for outdoor use and mobile applications.
"At L-com we strive to provide stellar wireless solutions for a variety of applications," said Kenneth Burgner, Product Manager, "And these new UR and MGUR mini antennas will be beneficial for several of those applications such as industrial complexes, public transportation, service vehicles, mobile wireless applications and more."
The first of the newly released series are the Dual Band 2.4/4.9-5.8 GHz Mini Mobile Mount antennas. The HG245803UR-NMOB and HG245803UR-NMOW are both compact 3 dBi omni-directional antennas designed primarily for multipoint and mobile applications in the 2.4 and 4.9-5.8 GHz frequency bands. Measuring only 2.7 inches long, these antennas feature a standard TAD/NMO-type connection.
The second set of products in the new series is the 698-960/1710-2700 MHz Mini Mobile Mount DAS antennas. The HG72703UR-NMOB and HG72703UR-NMOW are 3 dBi omni-directional antennas that have been specifically designed for use with DAS (Distributed Antenna Systems). They combine several different frequency bands to allow multi-user options. These compact antennas measure only 3.8 inches long and also feature a TAD/NMO type connection.
Both the antennas are also available as a kit with a magnetic mount. The MGUR series includes a chrome base with a heavy-duty magnet to ensure positive mounting. They are well suited for use in a range of mobile applications and solutions including service vehicles, public transportation, law enforcement, mining and construction vehicles. A 10-foot-high performance low-loss 195 series cable is provided and multiple connector options are also available.
For more information about this release, please contact:
Peter McNeil, Product Marketing Manager
978-682-6936 x1450, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###