NORTH ANDOVER, MA - 09/11/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, announced today that their most durable and rugged Cat5e cable line just got even tougher with the introduction of their new metal armored TRD8RGMT line.
These robust assemblies are constructed using L-com's IP68 ruggedized RJ45 plugs and jacks and feature crush resistant metal armor. They are designed for use in outdoor and industrial and military applications where the harshest environments exist.
"Harsh environments present many connectivity challenges. These include exposure to EMI/RFI, sun, moisture and chemicals," said David Gallagher, Product Manager. "Our new IP68 armored cable assemblies add to our wide variety of solutions for extreme network connectivity applications."
The six new cable assembly families from L-com are: TRD8RGMT1-, TRD8RGMT2-, TRD8RGMT3-, TRD8RGMT4-, TRD8RGMT5-, and TRD8RGMT6-. These assemblies use a Category 5e cable that is double shielded, high-flex, as well as UV and oil resistant. They are also made with a flame retardant thermoplastic elastomer (FR-TPE) jacket that is CMX outdoor rated. The metal armor protects the cable from impact damage and offers 1,500 pounds per square inch crush resistance.
Superior shielding of both the cable and connectors ensures higher data transmission rates up to gigabit Ethernet speeds. To suit every need, L-com also offers all plug and jack combinations off-the-shelf in both zinc nickel and anodized aluminum finishes.
For more information about this release, please contact:
Lindsey Cook, Internet Marketing Specialist
978-682-6936 x1148, lcook@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###