NORTH ANDOVER, MA – 12/1/2010 – L-com, Inc, a global leader in the manufacture of wired and wireless connectivity products, today announced the release of its DG9037 series of DB37 low profile right angle adapters. These adapters provide clearance in tight spaces by allowing cables to connect at a 90 degree angle.
L-com has been carrying 90 degree angle adapters for years, but this is the first adapter designed to accommodate the unusual DB37 connector, commonly used in complex instrumentation. Each adapter series comes in male to female and is available in “exit 1,” “exit 2,” and “exit 3” styles, allowing the cable to come off of the adapter in either direction. Hardware is reversible so either the male or female end will accept male thumbscrews or female standoffs. Please see the free tip for further exit orientation information.
L-com’s current list of right angle adapters now includes:
DB9 right angle adapters (exit 1, exit 2, and exit 3)
DB15 right angle adapters (exit 1, exit 2, and exit 3)
HD15 (VGA) right angle adapters (exit 1, exit 2, and exit 3)
DB25 right angle adapters (exit 1, exit 2, and exit 3)
DB37 right angle adapters (exit 1, exit 2, and exit 3)
Replacement 4-40 screws for right angle adapters
“Our right angle D-sub adapters are cost effective and efficient,” said Steve Smith, Product Manager, “and they remain very popular. I expanded this line because customers requested it.”
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.