NORTH ANDOVER, MA –03/23/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a bulk data cable with 20 AWG conductors, capable of carrying up to 10 amps per conductor. The new bulk cable is ideal for applications requiring higher current than is used with typical data systems.
“Customers were asking us for a bulk cable option that was more robust than typical 24 AWG cables,” said Steve Smith, Product Manager. “This new cable does the trick, and it broadens the spectrum of data cable capabilities.”
The new bulk cable has a braid and foil shield (double-shielded) for maximum EMI/RFI resistance. This UL2464-rated cable comes in 100-, 500-, and 1000-foot spools with either 9, 15, or 25 conductors.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/