NORTH ANDOVER, MA – 2/11/2010 – L-com Global Connectivity, a leading manufacturer of both wired and wireless connectivity products, released a “Universal” weatherproof enclosure. This new enclosure will handle 120VAC or 250VAC and can host a very large number of plug styles.
L-com originally manufactured this product for use in Europe with European style jacks. But the power module is designed to be removable, so you can install any jack that you may need.
The NBP141004-E00 also comes with these features:
- NEMA Type 3R / IP42 rated
- Made from rugged ABS
- Compact in size and can fit in tight spaces
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/