L-com's New 8x8 (RJ45) Plugs Designed to Terminate Large OD Conductors ![]() NORTH ANDOVER, MA - 01/25/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, now stocks an RJ45 (8x8) connector specifically designed to terminate conductors in a range of 0.044" to 0.048" (1.1 to 1.2 mm). It includes a metallic strain relief that accepts large OD cables of up to 0.310" (7.9 mm). The new plug is shielded, Category 6 rated for up to 1 Gbps transmission (and backwards compatible with Cat 5e and Cat 5), has a load bar for an easy termination and is sold either individually or in packages of 10. Most Category 6 plugs are designed to terminate on conductors that range from 0.037" to 0.042" (0.94 to 1.07mm). However, some heavy-duty industrial or outdoor rated cables, such as L-com's TFDL5089 bulk cable, utilize thicker conductors to improve a variety of factors such as flexibility and durability. These cables have typically required factory termination. L-com's new plug allows users to terminate their own cable assemblies at work sites or in the field. "Our customers were looking for a solution for using industrial bulk cable in situations where you can't pre-terminate the cable assembly," said David Gallagher, Product Manager. "We now offer such a solution." The new plug is stocked in L-com's North Andover, MA, distribution center for same day shipment. A detailed 2D engineering drawing is available for free download from L-com's web site. For a high-res version of the image suitable for print publication, please go to this link, right click on the image, and select Save As: https://www.l-com.com/lcom_emails/2013/012513/tsp8048c5s.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@L-com.com L-com, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |