L-com's New HyperLink® 90° Sector Panel Antennas for the 5 GHz Band are Dual Polarized ![]() NORTH ANDOVER, MA - 4/03/13 - L-com, Inc., a designer and manufacturer of wired and wireless connectivity products, has added a line of HyperLink® brand 90° sector panel antennas for the 5 GHz band that are dual polarized, offering high gain and wide bandwidth for IEEE 802.11a/n, 4.9 GHz Homeland Security, WiMAX and other applications. These DP series antennas can operate in vertical as well as horizontal polarization making them ideal for use with MIMO/802.11n multi-thread communication devices. L-com's new products feature heavy-duty UV-resistant plastic radomes for all-weather applications and come with stainless steel tilt-and-swivel mast mounting kits. The HG4958-17DP-90 offers 17 dBi gain in the 4.9-5.8 GHz band, while the HG5158-19DP-90 offers 19 dBi gain in the 5.1-5.8 GHz band. List prices start at $100US to $170US respectively, and quantity discounts are available for larger orders. "L-com now has a complete line up of HyperLink® high-gain dual polarized antennas that includes flat panels, parabolic dishes, and now sector panels," said Patrick Pesa, Director of Product Development. "We will continue to add new HyperLink® brand products to our offering to give our customers options for their applications." The new antennas are in stock and available for same-day shipment out of L-com's Boca Raton, FL, fulfillment center. Detailed 2D engineering drawings, 3D CAD models, and datasheets are available for free download from L-com's website. For a high-res version of the image suitable for print publication, please follow this link, right click on the image, and select Save As: https://www.l-com.com/lcom_emails/2013/040313/HG4958_17DP_090.jpg For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1169, dfallon@l-com.com L-com®, a global designer and manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the audio/video, OEM, military/aerospace, IT, and wireless RF industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the HyperLink® line of wireless antennas, amplifiers, filters/splitters, lightning protectors, weatherproof enclosures, and much more. Trusted for more than 30 years, L-com, Inc. is headquartered in North Andover, Massachusetts, USA, and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ ### |