NORTH ANDOVER, MA – 01/20/2010 – L-com Global Connectivity, a leading manufacturer of both wired and wireless connectivity products, announced today the release of their CAUALAL and CAUALB latching USB Cables. These cables feature a latching mechanism on the Type A male connector that insures a secure, strong connection even in any application.
The USB standard has been one of the most successful standards in connectivity history, despite some of its shortcomings. One of those shortcomings is that the connector traditionally is “friction fit”, and has a tendency to pull out of the mating jack when subject to light pressure or vibration.
L-com’s new latching USB products are expected to be very useful in high vibration applications, like in military and off-road vehicles, boats, and airplanes or anywhere that a “lost” connection is a problem.
This is not L-com’s first latching USB cable. In 2005, L-com introduced a coiling USB cable with latching Type A male connectors. These new cables come in various lengths and do not have the coiling feature.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized.
https://www.L-com.com/