NORTH ANDOVER, MA – 02/16/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now sells bulk USB 2.0 cable with a Low Smoke Zero Halogen (LSZH) jacket. The new product is identical to L-com’s standard PVC USB Bulk Cable, except that the jacket is black and, when burned, the LSZH jacket will not produce toxic smoke.
The USB Bulk Cable can be used with L-com’s Type A and Type B USB connectors and hoods to manufacture custom USB cables if desired. L-com can also manufacture custom USB cables using this bulk cable with modest minimum order quantities.
“All LSZH products appeal to military customers and military subcontractors because they significantly reduce the amount of toxic gases emitted during combustion when compared to PVC,” said Steve Smith, Product Manager. “This is essential for confined areas like aircraft, submarines and shipboard. This is the same cable that is used in our popular CSUZAB and CSUZAA cable assemblies.”
LSZH hoods for the connectors will be available in about six weeks.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/