L-com’s New Tool-Free D-Sub Connectors Simplify Field Termination NORTH ANDOVER, MA – July 28, 2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries a tool-free screwless version of its popular screw-down field termination connectors. The new connectors feature spring clamps instead of screws in the terminal block that allow easy termination of wires to a D-Sub connector in the field. “D-Sub connectors can be difficult to terminate,” said Steve Smith, product manager. “This new lineup will both simplify and speed up the process of field terminating D-Subs.” The new connectors are available in DB9, DB15, DB25, and HD15 versions. All of them are panel-mountable for thicknesses of up to 0.062”. For more information about this release, please contact: Dave Fallon, Internet Marketing Strategist 978-682-6936 x1450, newsletters@L-com.com L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as the Hyperlink line of wireless products. Trusted for more than 25 years, L-com, Inc. is headquartered in North Andover, Mass., and is ISO 9001: 2008-certified. For more information, please visit: https://www.L-com.com/ |