![]()
NORTH ANDOVER, MA - 12/18/14 - L-com Global Connectivity, a designer and manufacturer of wired and wireless connectivity products, now offers outdoor rated
Cat5e and
Cat6 cable assemblies for use in demanding outdoor Ethernet networking applications.
Gel-filled jackets provide moisture protection when used in outdoor environments and the UV protected jackets shield the cables from damage caused by sunlight exposure. Additionally, these cables are EIA568 color-coded for compatibility with standard installations and feature solid conductors for termination into standard IDC connectors.
"Our new outdoor rated Ethernet cables were designed to provide the basic features necessary for a cable to stand up to the elements. By utilizing UV protected jackets as well as Gel-filled cable construction we can ensure flawless operation even in the most demanding conditions." said Dave Gallagher, Product Manager. "These new assemblies are a great fit with our liquid tight cable glands which can be used at the demarcation points where the cables enter a building or enclosure." added Gallagher.
Both the Cat5e and Cat6 Outdoor cables are in stock and ready to ship. Custom lengths are also available upon request.
For more information about this release, please contact:
Peter McNeil, Marketing Manager
978-682-6936 x1174, pmcneil@l-com.com
About L-com Global Connectivity
L-com Global Connectivity, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their HyperLink® brand of wireless products which include antennas, RF amplifiers, coaxial lightning and surge protectors, and NEMA rated enclosures. L-com's HyperLink® wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n/ac, RFID and Bluetooth applications. In addition to HyperLink®, L-com's other brands include MilesTek®, specialists in Military/Aeronautics connectivity solutions and Aiconics®, a leading manufacturer of electrical connector products. Trusted for over 30 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized For more information, please visit: https://www.L-com.com/
###