NORTH ANDOVER, MA – 04/06/2011 – L-com, Inc., a global leader in the manufacture of wired and wireless connectivity products, now carries Round-It flexible split polyester tubing. Round-It’s self-wrapping feature allows for quick and easy application to and removal from cables, hoses or wire harnesses. The tough polyester material protects from chafing/cutting and allows for flexible routing. “Round-It is a perfect solution to reworking components without disconnecting them,” said Steve Smith, Product Manager. “This type of tubing is growing in popularity due to its easy application.”
The new tubing is only available in black, but comes in 5/16”, 0.5”, 1.0” and 1.5” diameters.
For more information about this release, please contact:
Dave Fallon, Internet Marketing Strategist
978-682-6936 x1450, newsletters@L-com.com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, Inc, which is headquartered in North Andover, MA, is ISO 9001: 2008 certified and many of its products are UL® recognized. https://www.L-com.com/