Adding to it’s Industrial Automation and networking offering, L-com Connectivity Products, of North Andover, MA now carries Multimode and Single Mode PROFIBUS and MODBUS media converters from Hirschmann Automation. As the need to support older field bus technologies increases more options for media connectivity are required in the industrial space. These hardened converters can connect to existing equipment such as PLC’s and support long distance fiber connections up to 15km.
These Hirschmann media converters join a broad line of both industrial and commercial media converters and other Hirschmann products that L-com has been offering for years. Along with both fiber and copper cable assemblies, IP67 rated cables, connectors, adapters, racks, panels and enclosures L-com boasts an impressive Industrial networking product line.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
- Assembled and Injection Molded Data Cables
- Fiber Optic Cable Assemblies and Adapters
- Modular and Telco Assemblies
- Low Loss Video and Monitor Cables
- Unique Bulkhead Connectors
- Machined or Cast Coaxial Connectors and Adapters
- Sheet Metal Fabrication of Rack Panels and Enclosures
- Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
- Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit http://www.L-com.com.