To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

L-com Carries Category 3 RJ12 110 Keystone Jacks For Telephone and Data Applications

Wednesday, July 11, 2007
North Andover, MA – July 12, 2007 – L-com Connectivity Products announced the addition of an RJ11/RJ12 Keystone style jack with 110 punch style terminals. This popular design allows fast and easy termination of telephone connections into wall plates that feature keystone style openings. The modular jack is available in two colors, ivory and white, and is color-coded for both EIA and USOC standards making it compatible with both old and new cabling installations.

This RJ11/RJ12 jack joins L-com's complete modular jack line. Wiring installers and integrators will often use these Keystone jacks in faceplates and panels. L-com is offering large volume quotations for installers and contractors looking to save money.

For more information about this release, please contact:
David Gallagher, Product Marketing Manager
978-682-6936 x127, dgallagher@L-com.com

For over 25 years, L-com Connectivity Products has designed, manufactured, and distributed an extensive offering of copper and fiber telecom and datacom interconnect components such as cable assemblies, adapters, couplers, and connectors, in addition to custom product design and manufacturing capabilities.  L-com is headquartered in North Andover, Massachusetts. For more information please visit www.L-com.com.