North Andover, MA, -- L-com Connectivity Products has introduced a line of IP66/67 rated industrial grade duplex LC fiber cable assemblies. L-com's new FODLC-IND series cables fearure IP66/67 rated duplex multimode LC connectors which stand up to harsh environments where dust, moisture, chemicals and other contaminants are present.
These industrial fiber assemblies feature robust strain relief connectors, which can handle in excess of 59 lbs of force, and rugged indoor/outdoor rated breakout style cable. This cable can be placed outdoors in a trough or conduit and is water resistant. In addition to several stocked lengths, L-com can manufacture custom industrial fiber cables to customers' exact specifications.
L-com designs and manufactures copper and fiber cable assemblies, interconnection adaptors, connectors and cable test equipment. In addition to a vast inventory of standard products, L-com has extensive custom product design and manufacturing capabilities that include:
- Assembled and Injection Molded Data Cables
- Fiber Optic Cable Assemblies and Adapters
- Modular and Telco Assemblies
- Low Loss Video and Monitor Cables
- Unique Bulkhead Connectors
- Machined or Cast Coaxial Connectors and Adapters
- Sheet Metal Fabrication of Rack Panels and Enclosures
- Special Bulk Cable Formulations (Low Smoke Zero Halogen, Ultra-Flexible, etc.)
- Military and Special Packaging, Kitting, Custom Labeling and Bar-coding
L-com also distributes selected products to complement its manufactured goods including: Ethernet hubs and switches, routers, media converters, protocol converters, KVM switches, video distribution amplifiers/switches and network test equipment. The company provides simple, one-stop shopping for its customers. For more information, please visit https://www.L-com.com
------------------------------------------------------------------------------------
L-com Connectivity Products 45 Beechwood Drive North Andover, MA 01845
www.L-com.com E-mail: sales@L-com.com Phone: 1-800-341-5266 Fax: 1-978-689-9484