IRVINE, Calif. (July 23, 2019) - L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new series of Cat5e, Cat6 and Cat6a patch panels for use in data center, LAN, MDF/IDF and Gigabit Ethernet connectivity applications.
L-com’s new patch panel line consists of panels with both standard keystone-style couplers as well as versions with L-com’s mini-couplers. Mini-couplers provide the same performance and quality as full-size Ethernet couplers, but measure less than one inch in length. This design provides more room for installers to work, improves air flow and reduces stress on cable exits, ensuring that the mating assembly’s bend radius is not exceeded. Additionally, many of these panels feature a cable management bar which is perfect for organizing and securing patch cables.
The new patch panels in this series include 24-port Cat5e, Cat6 and Cat6a V-Panels with cable management bar, 24 and 48-port Cat5e patch panels, 24 and 48-port Cat6 Ethernet cable patch panels, 24 and 48-port Cat6a patch panels, 24 and 48-port blank panels with keystone coupler cut outs and a 24-port Cat6 panel with right-angle couplers.
“This new patch panel series offers a wide range of options for our customers to address just about every telecom cable patching application. This new line ranges from 24 and 48-port, 1U and 2U panels to V-panels that are designed to reduce strain on installed connectors minimizing the need for rack mounted cable management bars in many network configurations,“ said Brian Gates, Product Manager.
L-com’s new patch panels are in-stock and available for immediate shipment.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2008 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, Kaelus, ShowMe Cables and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936
<!--[if gte mso 9]> <w:LsdException Locked=""false"" Priority=""50"" Name=""Grid Table 5 Dark Acce