IRVINE, Calif. L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of Ethernet cable assemblies that feature plenum-rated cable with a maximum temperature rating of +105°C.
L-com's new slim-line Cat6a and Cat6 Ethernet cable assemblies are the ideal solution for high density patching applications. The patent-pending, spline-free design provides a reduced diameter profile which offers a perfect solution for applications that require a smaller, more flexible cable.
Furthermore, L-com's low profile short boot design saves additional space on patch panels allowing for a clean organized installation. These CMP (plenum)-rated cables meet the most stringent of building burn and smoke codes. The stranded conductor design is considerably more flexible than a standard, solid conductor, horizontal cable with a greater flex life. A robust temperature range of -20°C to +105°C allows these cables to be used in higher temperature applications where standard patch cords would fail.
“Our new plenum-rated cable assemblies comply with stringent building codes by utilizing plenum-rated jackets. They limit the burn time and burn length compared to PVC cables and offer a wide operating temperature range for use in applications where extreme heat is present,” said Dustin Guttadauro, Product Manager.
In addition to these new cable assemblies, L-com also offers Cat6 and Cat6a plenum-rated bulk cable that is rated to +105°C.
L-com’s new plenum-rated Ethernet cables and bulk cable are in-stock and available for immediate shipment.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, Aiconics, KP Performance Antennas, PolyPhaser, Transtector, RadioWaves, Kaelus, ShowMe Cables and Integra Optics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, CA
978-682-6936