L-com, an Infinite Electronics brand and a preferred manufacturer of wired and wireless connectivity products, announced today that it has introduced a new line of low-PIM rated, ceiling, omni and flat panel antennas to address sub-6 GHz in-building connectivity.
L-com’s new 5G ceiling, omni antennas and flat panel antennas are perfect for use in indoor distributed wireless networks where support of sub-6 GHz 5G, LTE, FirstNet or other telecommunication networks are required. With multiple options for form factor, connector count and connector type, a full wireless network deployment can be achieved using these new antennas to reliably cover an entire building with high quality Wi-Fi/cellular service.
These new antennas feature 600 MHz to 6 GHz operation, less than -150 dBc PIM rating, SISO and 2x2 MIMO configurations. They also boast Type-N and 4.3-10 connector options, low-profile ceiling mounts for improved aesthetics, and compatibility with all global sub-6 GHz 5G bands including extended CBRS and UNII-1.
The HG7420-series antennas cover 698 MHz to 4200 MHz frequency bands and the HG6580-series supports 617 MHz to 6000 MHz wireless network applications.
"Our new 5G ceiling, omni and panel antennas were developed to address the latest 5G network deployments where high-performance along with low-PIM ratings are a requirement. By offering these new antennas as stock, off-the-shelf products, we are able to meet our customers’ installation deadlines,” said Kevin Hietpas, Product Line Manager.
L-com’s new low-PIM, 5G antennas and antenna connectors are in-stock and available for same-day shipping.
About L-com:
L-com, a leading manufacturer of wired and wireless connectivity products, offers a wide range of solutions and unrivaled customer service for the electronics and data communications industries. The company's product portfolio includes cable assemblies, connectors, adapters, antennas, enclosures, surge protectors and more. L-com is headquartered in North Andover, Mass., is ISO 9001: 2015 certified and many of its products are UL® recognized. L-com is an Infinite Electronics brand.
About Infinite Electronics:
Based in Irvine, Calif., Infinite Electronics offers a broad range of components, assemblies and wired/wireless connectivity solutions, serving the aerospace/defense, industrial, government, consumer electronics, instrumentation, medical and telecommunications markets. Infinite’s brands include Pasternack, Fairview Microwave, L-com, MilesTek, ShowMeCables, NavePoint, INC Installs, Integra Optics, PolyPhaser, Transtector, KP Performance Antennas, RadioWaves & Aiconics. Infinite Electronics serves a global engineering customer base with deep technical expertise and support, with one of the broadest inventories of products available for immediate shipment.
###
Press Contact:
Peter McNeil
L-com
17792 Fitch
Irvine, Calif. 92614
978-682-6936