To our valued customers please note that our offices and warehouses will be closed on the following date, December 25th, 2024 for the Christmas Holiday.
 
 

New DVI Products from L-com Support Growing A/V Market

Wednesday, March 18, 2009

NORTH ANDOVER, MA, -- March 17, 2009 -- L-com, a global leader in the manufacture of wired and wireless connectivity solutions, has released two new DVI products to support the growing A/V and Digital Signage industries.

The DVIDDLFT DVI-D Dual Link field termination connector is perfect for A/V installers who require the addition of DVI ports either in new or existing  installations. The DVIDDLFT can be installed in minutes using a standard Philips head screw driver. Furthermore the terminal block area is clearly marked making proper termination virtually foolproof.

 

In addition L-com has also released the new WPDVIFF stainless steel DVI wall plate. The WPDVIFF features a quality constructed female to female DVI adapter that is pre-mounted to the wall plate. This attractive and durable DVI wall plate is perfect for professional installers as well as do it yourselfers.

  
For more information about this release, please contact:

Greg Pepin, Product Manager
978-682-6936 x1186, gpepin@L-com.com


About L-com

 L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures.  L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.L-com.com