North Andover, MA – July 23, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity products today announced the release of two new USB products.
The USBAFT is a unique field terminate USB Type A connector that is designed to be used in the field for quick and easy terminations. Separate connection points are provided for all four positions of the connector plus the ground. Terminal block design with set screws provides reliable electrical connections utilizing no special tools. The terminal block area is clearly marked making proper termination virtually foolproof. The USBAFT is panel mountable using 4-40 screws provided
L-com's UADKEY-AB shielded USB keystone coupler can be easily installed into panels, wall plate openings and enclosures. The UADKEY-AB features a USB A female connector on the front and USB B female connector on the back of the coupler housing. The stamped metal shell and one piece design provides maximum protection from data corrupting EMI/RFI.
![]()
For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com