North Andover, MA – May 28, 2009 – L-com, a global leader in the manufacture of wired and wireless connectivity products today announced it now carries a flexible USB adapter that features vertical and horizontal hinges which allow the adapter to rotate in virtually any direction making it perfect for hard to reach or tight fit applications.
This flexible USB adapter is shielded to protect against data corrupting EMI/RFI and utilizes gold plating on all contacts to provide reliable connections with repeated mating cycles.
![]()
For more information about this release, please contact:
Steve Smith, Product Manager
978-682-6936 x1156, ssmith@L-com.com
About L-com
L-com, a global leader in the manufacture of wired and wireless connectivity products, offers a wide range of solutions and unmatched customer service for the electronics and data communications industries. The company’s product portfolio includes cable assemblies, connectors, adapters, computer networking components, and custom products, as well as their Hyperlink line of wireless products which include Antennas, RF Amplifiers, Coaxial lightning and surge protectors, and NEMA rated enclosures. L-com’s HyperLink wireless products are designed for WiFi, WiMAX, SCADA, 802.11a/b/g/n, RFID and Bluetooth applications. Trusted for over 25 years, L-com, which is headquartered in North Andover, MA, is ISO 9001: 2000 certified and many of its products are UL® recognized. www.l-com.com